In action across the globe


Photo: fotolia

Pyramid of Cheops

In the access shaft of the Pyramid of Cheops, salt-resistant
Lapp ÖLFLEX® cables ensure the air conditioning system of
this wonder of the world operates smoothly.

 


Singapore Flyer

Towering to a height of 178 m and with a diameter of 150 m,
the Singapore Flyer is the ultimate visitor attraction in Singapore.
What’s more, the over 30 km of halogen-free ÖLFLEX® cables will
release no toxic fumes in the event of fire.
 


Photo: Singapur Flyer Pte Ltd



Foto: Lapp Kabel Stuttgart

Radiotelescope Effelsberg

Bad Münstereifel is home to the Effelsberg radio
telescope, one of the largest of its kind. The motors
that steer the telescope are powered using ÖLFLEX®
connection and control cables.


Europa-Park Rust

More and more fairground rides across the globe are
putting their trust in ÖLFLEX® cables. And with good reason –
after all, safety always comes first.


Photo: Europapark Rust



Photo: Multibrid GmbH

Wind Turbines

ÖLFLEX® cables are installed in many wind turbines.
ÖLFLEX® WIND is a cable specially designed to deal with
the high torsional forces that occur at the crossover from
the nacelle to the tower.
 


Solar

The solar park in Bovera, Spain, covers 24,700 m2, contains
5,400 solar modules and generates 1,440 megawatt
hours of electricity. 20 km of ÖLFLEX® SOLAR
cables were installed here to ensure the park operates
perfectly.
 

 


Photo: Wirsol Solar AG



Photo: Dürr AG

Roboter

ÖLFLEX® ROBOT cables are not only highly flexible,
they are also torsionresistant. This makes them ideal
for operating industrial robots. 

 


Paper Manufacturing

When it comes to largescale paper manufacturing
machines, a range of ÖLFLEX® cables ensures
that everything works just as it should!


Photo: Fa. Voith

Lapp Company Finder
Find a Lapp contact in your Country!
A cable conquers the world


ÖLFLEX® 50 Movie
Lapp Insulator is not affiliated with the Lapp Group.